MITSUBISHI ELECTRIC Changes for the Better
Machine Building

Connectivity in modern machinery

02.11.20263 minuters läsning

Digital transformation is making machine connectivity a key requirement for modern manufacturing. Connected equipment helps manufacturers improve productivity, minimise downtime, and gain greater visibility into production processes. By linking machines, control systems, and software platforms, operational data can be transformed into actionable insights that support continuous improvement.

Which machine data should manufacturers connect and why?

The most valuable connectivity strategies focus on data that supports performance, maintenance, and quality improvements. Common examples include production output, machine availability, alarm information, energy consumption, and quality-related metrics.

Connected Data TypeBusiness Value
Machine statusImproved visibility and uptime
Alarm dataFaster troubleshooting
Energy usageReduced operating costs
Performance metricsHigher productivity
Quality dataImproved product consistency

When analysed together, these data sources provide a clearer picture of machine performance and production efficiency. This enables manufacturers to optimise operations, improve resource utilisation, and support predictive maintenance initiatives.

How can machine builders connect controllers, drives and other machine components?

Modern machines combine PLCs, robotics, motion systems, HMIs, sensors, and safety devices. To ensure efficient communication between these components, machine builders increasingly adopt integrated automation architectures that support data exchange across the machine and beyond.

Mitsubishi Electric supports this approach through its machine building solutions, helping OEMs create scalable and future-ready machines while simplifying system integration and reducing engineering complexity.

How can connectivity be added to existing machinery?

Legacy equipment can often be connected without major modifications. Communication modules, industrial networking technologies, and edge-level solutions allow manufacturers to access operational data from existing assets and integrate them into modern digital environments.

Retrofitting machinery offers a practical and cost-effective path to digital transformation while preserving previous investments. It also enables manufacturers to improve production visibility and make better use of installed equipment.

How can connected machines support remote monitoring and maintenance?

Remote connectivity gives maintenance teams access to machine information without being physically present on site. Operational data can be analysed in real time, supporting faster diagnostics and more effective maintenance planning.

Key benefits include:

  • reduced downtime,
  • faster fault resolution,
  • improved maintenance efficiency,
  • lower support costs,
  • greater machine availability.

By identifying issues before they lead to failures, manufacturers can move from reactive maintenance towards a more proactive approach that improves reliability and productivity.

    What should OEMs consider when choosing a machine connectivity architecture?

    Machine builders should ensure that connectivity solutions support:

    • scalability,
    • interoperability,
    • cybersecurity,
    • standards compliance,
    • long-term maintainability.

    Connectivity architectures should also be flexible enough to support future expansion and evolving production requirements. These priorities align with Mitsubishi Electric's four pillars of machine building approach, which focuses on flexibility, efficiency, scalability, and long-term value.

      How can manufacturers manage connectivity across machines from different suppliers?

      Most factories operate equipment from multiple vendors, making connectivity a key consideration when modernising production environments. Different machine generations, communication methods, and software platforms can create data silos that limit visibility.

      A well-designed connectivity strategy enables information to be shared across machines and production systems, helping manufacturers improve operational efficiency and make more informed decisions. Solutions from Mitsubishi Electric support the integration of diverse production assets, enabling organisations to build connected environments that support productivity improvements, maintenance optimisation, and long-term scalability.

      Sources:

      • OPC Foundation – OPC UA for Machinery
        https://opcfoundation.org/markets-collaboration/opc-ua-for-machinery/
      •  VDMA – Interoperability
        https://www.vdma.eu/en/interop...
      • ISA – IIoT Remote Monitoring
        https://www.isa.org/intech-hom...

      FAQ section

      What does machine connectivity mean in manufacturing?

      Machine connectivity refers to the ability of production equipment, controllers, drives, sensors, software, and enterprise systems to exchange data through wired or wireless communication networks.

      How do connected machines share data with production systems?

      Connected machines typically use industrial communication protocols such as OPC UA, MQTT, PROFINET, EtherNet/IP, or CC-Link IE to transmit operational data to SCADA, MES, ERP, cloud, or analytics platforms.

      Can older machines be connected to a modern industrial network?

      Yes. Gateways, protocol converters, communication modules, and edge devices can enable legacy equipment to participate in modern connectivity architectures.

      Do connected machines need a cloud connection?

      No. Many implementations process and analyse data locally using on-premises infrastructure or edge computing platforms. Cloud connectivity remains optional depending on operational requirements.

      What should machine builders consider before connecting a machine?

      Machine builders should evaluate cybersecurity, interoperability, scalability, data ownership, communication standards, performance requirements, and long-term maintainability when designing connected machines.


      Liknande artiklar


      Ämnen

      Machine Building